6.20.14 strerror Function
Gets an internal error message.
Include
<string.h>
Prototype
char *strerror(int errcode);
Argument
errcode- number of the error code
Return Value
Returns a pointer to an internal error message string corresponding to the specified
error code errcode.
Remarks
| Error condition | String |
|---|---|
EILSEQ | "Illegal byte sequence" |
EDOM | "Domain error" |
ERANGE | "Result not representable" |
EOVERFLOW | "Value too large for data type" |
EINVAL | "Invalid argument" |
0 | "No error information" |
The array pointed to by strerror may be overwritten by a subsequent call
to this function, so it is not thread safe.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <string.h>
#include <math.h>
#include <stdio.h>
#include <errno.h>
int main()
{
double result, x=-9.0;
result = log(x);
if(errno)
printf("Log generated %s\n", strerror(errno));
else
printf("Log of %g is %g\n", x, result);
}Example Output
Log generated Mathematics argument out of domain of function