36.6.11 ISI Status Register
| Name: | ISI_SR |
| Offset: | 0x28 |
| Reset: | 0x00000000 |
| Property: | Read-only |
| Bit | 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | |
| FR_OVR | CRC_ERR | C_OVR | P_OVR | ||||||
| Access | R | R | R | R | |||||
| Reset | 0 | 0 | 0 | 0 |
| Bit | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | |
| SIP | CXFR_DONE | PXFR_DONE | |||||||
| Access | R | R | R | ||||||
| Reset | 0 | 0 | 0 |
| Bit | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | |
| VSYNC | CDC_PND | ||||||||
| Access | R | R | |||||||
| Reset | 0 | 0 |
| Bit | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 | |
| SRST | DIS_DONE | ENABLE | |||||||
| Access | R | R | R | ||||||
| Reset | 0 | 0 | 0 |
Bit 27 – FR_OVR Frame Rate Overrun (cleared on read)
| Value | Description |
|---|---|
| 0 | No frame overrun |
| 1 | Frame overrun. The current frame is being skipped because a vsync signal has been detected while flushing FIFOs since the last read of ISI_SR. |
Bit 26 – CRC_ERR CRC Synchronization Error (cleared on read)
| Value | Description |
|---|---|
| 0 | No CRC error in the embedded synchronization frame (SAV/EAV) |
| 1 | Embedded Synchronization Correction is enabled (CRC_SYNC bit is set) in the ISI_CR and an error has been detected and not corrected since the last read of ISI_SR. The frame is discarded and the ISI waits for a new one. |
Bit 25 – C_OVR Codec Datapath Overflow (cleared on read)
| Value | Description |
|---|---|
| 0 | No overflow |
| 1 | An overrun condition has occurred in input FIFO on the codec path. The overrun happens when the FIFO is full and an attempt is made to write a new sample to the FIFO since the last read of ISI_SR. |
Bit 24 – P_OVR Preview Datapath Overflow (cleared on read)
| Value | Description |
|---|---|
| 0 | No overflow |
| 1 | An overrun condition has occurred in input FIFO on the preview path. The overrun happens when the FIFO is full and an attempt is made to write a new sample to the FIFO since the last read of ISI_SR. |
Bit 19 – SIP Synchronization in Progress
When the status of the preview or codec DMA channel is modified, a minimum amount of time is required to perform the clock domain synchronization.
| Value | Description |
|---|---|
| 0 | The clock domain synchronization process is terminated. |
| 1 | This bit is set when the clock domain synchronization operation occurs. No modification of the channel status is allowed when this bit is set, to guarantee data integrity. |
Bit 17 – CXFR_DONE Codec DMA Transfer has Terminated (cleared on read)
| Value | Description |
|---|---|
| 0 | Codec transfer done not detected. |
| 1 | Codec transfer done detected. When set, this bit indicates that the data transfer on the codec channel has completed since the last read of ISI_SR. |
Bit 16 – PXFR_DONE Preview DMA Transfer has Terminated (cleared on read)
| Value | Description |
|---|---|
| 0 | Preview transfer done not detected. |
| 1 | Preview transfer done detected. When set, this bit indicates that the data transfer on the preview channel has completed since the last read of ISI_SR. |
Bit 10 – VSYNC Vertical Synchronization (cleared on read)
| Value | Description |
|---|---|
| 0 | Indicates that the vertical synchronization has not been detected since the last read of the ISI_SR. |
| 1 | Indicates that a vertical synchronization has been detected since the last read of the ISI_SR. |
Bit 8 – CDC_PND Pending Codec Request
| Value | Description |
|---|---|
| 0 | Indicates that no codec request is pending |
| 1 | Indicates that the request has been taken into account but cannot be serviced within the current frame. The operation is postponed to the next frame. |
Bit 2 – SRST Module Software Reset Request has Terminated (cleared on read)
| Value | Description |
|---|---|
| 0 | Indicates that the request is not completed (if a request was issued). |
| 1 | Software reset request has completed. This flag is reset after a read operation. |
Bit 1 – DIS_DONE Module Disable Request has Terminated (cleared on read)
| Value | Description |
|---|---|
| 0 | Indicates that the request is not completed (if a request was issued). |
| 1 | Disable request has completed. This flag is reset after a read operation. |
Bit 0 – ENABLE Module Enable
| Value | Description |
|---|---|
| 0 | Module is disabled. |
| 1 | Module is enabled. |