5.5 LED Driver
The IS2062GM and IS2064B have two LED drivers, and the IS2064GM and IS2064S have three LED drivers to control the LEDs. The LED drivers provide enough sink current (16-step control and 0.35 mA for each step) and the LED is connected directly to the IS2062/64 SoC. The LED settings are configured using the UI tool.
The following figure illustrates the LED driver in the IS2062/64 SoC.