8.2.2 Internal Clock Sources
The device may be configured to use the internal oscillator block as the system clock by performing one of the following actions:
- Program the RSTOSC bits in Configuration Word 1 to select the INTOSC clock source, which will be used as the default system clock upon a device Reset.
- Write the NOSC bits to switch the system clock source to the internal oscillator during run-time.
The function of the OSC2/CLKOUT pin is determined by the CLKOUTEN bit in Configuration Word 1.
The internal oscillator block has two independent oscillators that can produce two internal system clock sources.
- The HFINTOSC (High-Frequency Internal Oscillator) is factory-calibrated and operates up to 32 MHz.
- The LFINTOSC (Low-Frequency Internal Oscillator) is factory-calibrated and operates at 31 kHz.