37.2.4.4.1 Transmit Buffer and FIFO Operation
The I3CxTXB register is safe to write when the contents of the register is empty. This condition is represented through the Transmit Buffer Empty TXBE bit. This also results in the I3CxTXIF system level interrupt flag being set, which can also be used as a DMA trigger.
When the user software writes data to the I3CxTXB register, the TXBE and I3CxTXIF bits are
cleared. The data are then passed onto the Transmit FIFO, which sets the Transmit FIFO Not
Empty TXFNE bit and,
subsequently, the TXBE/I3CxTXIF bits as well. If the data are written to the I3CxTXB Transmit
Buffer faster than the Controller’s reading speed, it is possible that the Transmit Buffer and
FIFO will eventually become full and the TXBE and I3CxTXIF bits will remain cleared,
signifying that the I3CxTXB register cannot accept new data. If the I3CxTXB Transmit Buffer is
written to when it is full (TXBE =
0), a Transmit Buffer Write Error occurs
and the TXWEIF
interrupt flag is set. The TXBE and I3CxTXIF flags are set again as soon as the Controller
reads from the Transmit FIFO and the data in the I3CxTXB register are shifted into the
Transmit FIFO. The TXFNE bit is cleared after all the data in the Transmit FIFO have been
transmitted on the bus or a buffer reset operation has been performed using the CLRTXB bit. It is also possible that the Controller attempts to read from the Target
when the Transmit FIFO is empty (TXFNE = 0), in which case a Transmit Underrun occurs, the
TXUIF interrupt flag is set, and the read request is NACKed by the Target.| I3CxTXB Transmit Buffer Status | Transmit FIFO Status | TXBE/I3CxTXIF | TXFNE | Other Interrupts |
|---|---|---|---|---|
| Empty | Empty | 1 | 0 | TXUIF is set when read is requested by the Controller(1) |
| Full | Empty | 0 | 0 | TXUIF is set when read is requested by the Controller(1) TXWEIF is set when write is attempted to the I3CxTXB register |
| Empty | Partially Full or Full | 1 | 1 | |
| Full | Partially Full or Full | 0 | 1 | TXWEIF is set when write is attempted to the I3CxTXB register |
Note:
| ||||
Important:
- While the Target will typically continue to
transmit data (with End-of-Data T-bit =
1) during a Private Read or IBI transaction as long the Transmit FIFO is not empty (TXFNE =1), the transmit operation can be limited if the Maximum Read Length (I3CxMRL register) or IBI Payload Size Limit (I3CxIBIPSZ register) is set. When the Maximum Read Length or the IBI Payload Size Limit has been reached in the appropriate transaction, the Target will stop transmitting further data (with End-of-Data T-bit =0) even if the Transmit FIFO is not empty. This does not affect the operation of other Transmit Status and Interrupt flags. - This Target module will always NACK an
I2C/Private Read request when the Transmit FIFO is empty (TXFNE =
0). When data are available in the Transmit FIFO (TXFNE =1), the Target module will ACK an I2C/Private Read request when the ACKP bit =0. To NACK an I2C/Private Read request when data are in the Transmit FIFO, the ACKP bit must be set to1. With ACKP bit set, a one-time ACK can be performed using the ACKPOS bit. Refer to Private Read Transaction for more information.