4.28.7 TSN PSFP Stream Filter Configuration
The TSN PSFP Stream Filter Configuration page has the following parameters:
- Delete: Click to delete the entry. It will be deleted during the next save.
- SFI ID: The Stream Filter Instance parameter is an index into the Stream Filter Table.
- Stream ID: The Stream Handle Spec parameter contains a stream identifier specification value. A value of -1 denotes the wild card value; all positive values denote stream identifier values.
- Priority Spec: The Priority Spec parameter contains a priority specification value. A value of -1 denotes the wild card value; zero or positive values denote priority values.
- Interface Spec: The Interface Spec parameter contains an interface specification value. A value of VTSS_IFINDEX_NONE denotes the wild card value.
- SGI ID: The Stream Gate Instance parameter contains the index of an entry in the Stream Gate Table.
- SDU Size: The Maximum SDU Size parameter specifies the maximum allowed frame size for the stream. Any frame exceeding this value will be dropped. A value of 0 denote that the Maximum SDU Size filter is disabled for this stream.
- FMI ID: The Flow Meter Instance ID parameter contains the index of an entry in the Flow Meter Table. A value of -1 denotes that no flow meter is assigned; zero or positive values denote flow meter IDs.
- Block Oversize Enable: The Stream Blocked Due To Oversize Frame Enable object contains a Boolean value that indicates whether the Stream Blocked Due To Oversize Frame function is enabled (TRUE) or disabled (FALSE).
- Block Oversize: The Stream Blocked Due To Oversize Frame object contains a Boolean value that indicates whether, if the Stream Blocked Due To Oversize Frame function is enabled, all frames are to be discarded (TRUE) or not (FALSE).