4.28.8 TSN PSFP Stream Gate Configuration
The TSN PSFP Stream Gate Configuration page has the following parameters:
- Delete: Click to delete the entry. It will be deleted during the next save.
- SGI ID: The Stream Gate Instance parameter is an index into the Stream Gate Table.
- Gate Enabled: The Gate Enabled parameter determines whether the stream gate is active (true) or inactive (false).
- Gate States: The administrative value of the Gate States parameter for the stream gate. The open value indicates that the gate is open, the closed value indicates that the gate is closed.
- Cycle Time Value: The administrative value of the cycle time for the gate. The time may be specified in either milliseconds, microseconds or nanoseconds as defined by the field Cycle Time unit.
- Cycle Time unit: The unit used for specifying the administrative cycle time. Possible values are ns, us or ms.
- Cycle Time Extension: The administrative value of the Cycle Time Extension parameter for the gate. The value is an unsigned integer number of nanoseconds.
- Base Time: The administrative value of the Base Time parameter for the gate. The value is a representation of a PTPtime value, consisting of decimal number of seconds since epoch. The time can be given with a resolution of nine decimals.
- Admin IPV: The administrative value of the IPV parameter for the gate. A value of -1 denotes the null value.
- GCL Length: The number of entries in the Gate Control List.
- GCL Configuration: Configuration of the Gate Control List.
- Enable Gate-closed-due-to invalid-rx: A Boolean value that indicates whether to close the gate if invalid data is received.
- Enable Gate-closed-due-to octets-exceeded: A Boolean value that indicates whether to close the gate if too many octets are received
- Config Change: The Config Change parameter signals the start of a configuration change for the gate when it is set to TRUE. This should only be done when the various administrative parameters are all set to appropriate values.