4.28.6 TSN PSFP Flow Meter Configuration
The TSN PSFP Flow Meter Configuration page has the following parameters:
- Delete: Click to delete the entry. It will be deleted during the next save.
- FMI ID: The Flow Meter Instance (FMI) parameter is an index into the Flow Meter Table.
- CIR: The Flow Meter CIR parameter contains an integer value that represents the CIR value for the flow meter, in bit/s.
- CBS: The Flow Meter CBS parameter contains an integer value that represents the CBS value for the flow meter, in octets.
- Mark RED Enable: The Flow Meter Mark All Frames Red Enable parameter contains a Boolean value that indicates whether the Mark All Frames Red function is enabled (TRUE) or disabled (FALSE).
- Mark RED: The Flow Meter Mark All Frames Red parameter contains a Boolean value that indicates whether, if the Mark All Frames Red function is enabled, all frames are to be discarded (TRUE) or not (FALSE).