4.28.2 TSN PTP Check Configuration
The TSN PTP Check Configuration page has the following parameters:
When using TAS and PSFP between network elements, it is required to have a common global time reference provided by PTP. When booting the device, it will take some time for a configured PTP application to get locked to the common time reference. It may cause malfunctioning of TAS and PSFP if config-change is issued before PTP time is in a Locked or Locking state. A function which can delay the issue of config-change until PTP is Locked/Locking or a configurable time has passed, can be configured here.
- Procedure: Select how to ensure PTP state.
- Timeout: Specify the maximal number of seconds to wait before config_change is issued.
- PTPport: Specify the PTP port to use for sensing PTP status