7.1 Tera Term Setup
(Ask a Question)The user application provides a user interface on the Tera Term terminal through the UART interface.
To setup the Tera Term program, perform the following steps:
- Ensure that the USB cable connects the host PC to the J5 (USB) port on the PolarFire Evaluation board.
- Start Tera Term.
- Select Serial as the Connection type.
- Set the serial
Port to the second highest COM port number from the drop-down
list as shown in the following figure. For example, COM33: FlashPro5 Port
[COM33] in this instance.
Figure 7-1. Select Serial as the Connection Type 
- In the Tera Term
window, go to Setup > Serial port..., set Baud
rate to 115200.
Rest of the serial port settings must be at default state as shown in the following figure and click OK.
Figure 7-2. Tera Term Configuration 
- In the Tera Term
window, go to Setup > General..., set the
Language to English and click
OK, as shown in the following figure. This setup is required
for running the Tera Term macro script.
Figure 7-3. Tera Term General Setup 
This completes the Tera Term program setup.