12 Revision History

The revision history describes the changes that were implemented in the document. The changes are listed by revision, starting with the most current publication.

RevisionDateDescription
D02/2024Added a note in the DDR3 section.
C10/2023

The following is the list of changes in revision C of the document:

B06/2022

The following is the list of changes in revision B of the document:

A06/2022

The following is the list of changes in revision A of the document:

4.0—

Added Appendix 4: Running the TCL Script.

3.0—

The following is a summary of the changes made in this revision.

  • Updated the document for Libero® SoC v12.2.
  • Removed the references to Libero version numbers.
2.0—

The document was updated for Libero SoC v12.0 release.

1.0—Initial Revision.