25.6.4.11.1 Function tcc_set_ramp_index()
Sets the TCC module ramp index on next cycle.
void tcc_set_ramp_index( const struct tcc_module *const module_inst, const enum tcc_ramp_index ramp_index)
In RAMP2 and RAMP2A operation, we can force either cycle A or cycle B at the output, on the next clock cycle. When ramp index command is disabled, cycle A and cycle B will appear at the output, on alternate clock cycles. See tcc_ramp.
| Data direction | Parameter name | Description |
|---|---|---|
[in] | module_inst |
Pointer to the software module instance struct |
[in] | ramp_index |
Ramp index (tcc_ramp_index) of the next cycle |