25.8.6.1.2 Code
Add to the main application source file, before any functions, according to the kit used:
- SAM D21 Xplained Pro.
#define CONF_PWM_MODULE LED_0_PWM4CTRL_MODULE#define CONF_PWM_CHANNEL LED_0_PWM4CTRL_CHANNEL#define CONF_PWM_OUTPUT LED_0_PWM4CTRL_OUTPUT#define CONF_PWM_OUT_PIN LED_0_PWM4CTRL_PIN#define CONF_PWM_OUT_MUX LED_0_PWM4CTRL_MUX#define CONF_FAULT_EIC_PIN SW0_EIC_PIN#define CONF_FAULT_EIC_PIN_MUX SW0_EIC_PINMUX#define CONF_FAULT_EIC_LINE SW0_EIC_LINE#define CONF_FAULT_EVENT_GENERATOR EVSYS_ID_GEN_EIC_EXTINT_15#define CONF_FAULT_EVENT_USER EVSYS_ID_USER_TCC0_MC_0 - SAM R21 Xplained Pro.
#define CONF_PWM_MODULE TCC1#define CONF_PWM_CHANNEL 0#define CONF_PWM_OUTPUT 0#define CONF_PWM_OUT_PIN PIN_PA06E_TCC1_WO0#define CONF_PWM_OUT_MUX MUX_PA06E_TCC1_WO0#define CONF_FAULT_EIC_PIN SW0_EIC_PIN#define CONF_FAULT_EIC_PIN_MUX SW0_EIC_PINMUX#define CONF_FAULT_EIC_LINE SW0_EIC_LINE#define CONF_FAULT_EVENT_GENERATOR EVSYS_ID_GEN_EIC_EXTINT_8#define CONF_FAULT_EVENT_USER EVSYS_ID_USER_TCC1_MC_0 - SAM L21 Xplained Pro.
#define CONF_PWM_MODULE LED_0_PWM4CTRL_MODULE#define CONF_PWM_CHANNEL LED_0_PWM4CTRL_CHANNEL#define CONF_PWM_OUTPUT LED_0_PWM4CTRL_OUTPUT#define CONF_PWM_OUT_PIN LED_0_PWM4CTRL_PIN#define CONF_PWM_OUT_MUX LED_0_PWM4CTRL_MUX#define CONF_FAULT_EIC_PIN SW0_EIC_PIN#define CONF_FAULT_EIC_PIN_MUX SW0_EIC_PINMUX#define CONF_FAULT_EIC_LINE SW0_EIC_LINE#define CONF_FAULT_EVENT_GENERATOR EVSYS_ID_GEN_EIC_EXTINT_2#define CONF_FAULT_EVENT_USER EVSYS_ID_USER_TCC0_MC_0 - SAM L22 Xplained Pro.
#define CONF_PWM_MODULE TCC0#define CONF_PWM_CHANNEL 0#define CONF_PWM_OUTPUT 0#define CONF_PWM_OUT_PIN PIN_PB18F_TCC0_WO0#define CONF_PWM_OUT_MUX MUX_PB18F_TCC0_WO0#define CONF_FAULT_EIC_PIN SW0_EIC_PIN#define CONF_FAULT_EIC_PIN_MUX SW0_EIC_PINMUX#define CONF_FAULT_EIC_LINE SW0_EIC_LINE#define CONF_FAULT_EVENT_GENERATOR EVSYS_ID_GEN_EIC_EXTINT_9#define CONF_FAULT_EVENT_USER EVSYS_ID_USER_TCC0_MC_0 - SAM DA1 Xplained Pro.
#define CONF_PWM_MODULE LED_0_PWM4CTRL_MODULE#define CONF_PWM_CHANNEL LED_0_PWM4CTRL_CHANNEL#define CONF_PWM_OUTPUT LED_0_PWM4CTRL_OUTPUT#define CONF_PWM_OUT_PIN LED_0_PWM4CTRL_PIN#define CONF_PWM_OUT_MUX LED_0_PWM4CTRL_MUX#define CONF_FAULT_EIC_PIN SW0_EIC_PIN#define CONF_FAULT_EIC_PIN_MUX SW0_EIC_PINMUX#define CONF_FAULT_EIC_LINE SW0_EIC_LINE#define CONF_FAULT_EVENT_GENERATOR EVSYS_ID_GEN_EIC_EXTINT_15#define CONF_FAULT_EVENT_USER EVSYS_ID_USER_TCC0_MC_0 - SAM C21 Xplained Pro:
#define CONF_PWM_MODULE LED_0_PWM4CTRL_MODULE#define CONF_PWM_CHANNEL LED_0_PWM4CTRL_CHANNEL#define CONF_PWM_OUTPUT LED_0_PWM4CTRL_OUTPUT#define CONF_PWM_OUT_PIN LED_0_PWM4CTRL_PIN#define CONF_PWM_OUT_MUX LED_0_PWM4CTRL_MUX
Add to the main application source file, before any functions:#define CONF_FAULT_EIC_PIN SW0_EIC_PIN#define CONF_FAULT_EIC_PIN_MUX SW0_EIC_PINMUX#define CONF_FAULT_EIC_LINE SW0_EIC_LINE#define CONF_FAULT_EVENT_GENERATOR EVSYS_ID_GEN_EIC_EXTINT_8#define CONF_FAULT_EVENT_USER EVSYS_ID_USER_TCC0_EV_0
Add to the main application source file, outside of any functions:#include <string.h>structtcc_module tcc_instance;
Copy-paste the following callback function code to your user application:structevents_resource event_resource;staticvoidtcc_callback_to_change_duty_cycle(structtcc_module *constmodule_inst){staticuint32_t delay = 10;staticuint32_t i = 0;if(--delay) {return;}delay = 10;i = (i + 0x0800) & 0xFFFF;tcc_set_compare_value(module_inst,(enumtcc_match_capture_channel)(TCC_MATCH_CAPTURE_CHANNEL_0 + CONF_PWM_CHANNEL),i + 1);}
Copy-paste the following setup code to your user application:staticvoideic_callback_to_clear_halt(void){if(port_pin_get_input_level(CONF_FAULT_EIC_PIN)) {tcc_clear_status(&tcc_instance,TCC_STATUS_RECOVERABLE_FAULT_OCCUR(CONF_PWM_CHANNEL));}}staticvoidconfigure_tcc(void){structtcc_config config_tcc;tcc_get_config_defaults(&config_tcc, CONF_PWM_MODULE);config_tcc.counter.period = 0xFFFF;config_tcc.compare.wave_generation = TCC_WAVE_GENERATION_SINGLE_SLOPE_PWM;config_tcc.compare.match[CONF_PWM_CHANNEL] = 0xFFFF;config_tcc.wave_ext.recoverable_fault[CONF_PWM_CHANNEL].source =TCC_FAULT_SOURCE_ENABLE;config_tcc.wave_ext.recoverable_fault[CONF_PWM_CHANNEL].halt_action =TCC_FAULT_HALT_ACTION_SW_HALT;config_tcc.pins.enable_wave_out_pin[CONF_PWM_OUTPUT] =true;config_tcc.pins.wave_out_pin[CONF_PWM_OUTPUT] = CONF_PWM_OUT_PIN;config_tcc.pins.wave_out_pin_mux[CONF_PWM_OUTPUT] = CONF_PWM_OUT_MUX;tcc_init(&tcc_instance, CONF_PWM_MODULE, &config_tcc);structtcc_events events;memset(&events, 0,sizeof(structtcc_events));events.on_event_perform_channel_action[CONF_PWM_CHANNEL] =true;tcc_enable_events(&tcc_instance, &events);tcc_enable(&tcc_instance);}staticvoidconfigure_tcc_callbacks(void){tcc_register_callback(&tcc_instance,tcc_callback_to_change_duty_cycle,(enumtcc_callback)(TCC_CALLBACK_CHANNEL_0 + CONF_PWM_CHANNEL));tcc_enable_callback(&tcc_instance,(enumtcc_callback)(TCC_CALLBACK_CHANNEL_0 + CONF_PWM_CHANNEL));}staticvoidconfigure_eic(void){structextint_chan_conf config;extint_chan_get_config_defaults(&config);config.filter_input_signal =true;config.detection_criteria = EXTINT_DETECT_BOTH;config.gpio_pin = CONF_FAULT_EIC_PIN;config.gpio_pin_mux = CONF_FAULT_EIC_PIN_MUX;extint_chan_set_config(CONF_FAULT_EIC_LINE, &config);structextint_events events;memset(&events, 0,sizeof(structextint_events));events.generate_event_on_detect[CONF_FAULT_EIC_LINE] =true;extint_enable_events(&events);extint_register_callback(eic_callback_to_clear_halt,CONF_FAULT_EIC_LINE, EXTINT_CALLBACK_TYPE_DETECT);extint_chan_enable_callback(CONF_FAULT_EIC_LINE,EXTINT_CALLBACK_TYPE_DETECT);}
Add to user application initialization (typically the start of main()):staticvoidconfigure_event(void){structevents_config config;events_get_config_defaults(&config);config.generator = CONF_FAULT_EVENT_GENERATOR;config.path = EVENTS_PATH_ASYNCHRONOUS;events_allocate(&event_resource, &config);events_attach_user(&event_resource, CONF_FAULT_EVENT_USER);}configure_tcc();configure_tcc_callbacks();configure_eic();configure_event();