24.6.4.5.1 Function tc_stop_counter()
Stops the counter.
void tc_stop_counter( const struct tc_module *const module_inst)
This function will stop the counter. When the counter is stopped the value in the count value is set to 0 if the counter was counting up, or maximum if the counter was counting down when stopped.
| Data direction | Parameter name | Description |
|---|---|---|
[in] | module_inst |
Pointer to the software module instance struct |