3.6 Bluetooth® Low Energy Peripheral Connection
This section helps users enable advertisements and connection on the Curiosity board using the MCC. The peripheral device will be the Curiosity board and the central device can either be a smart phone with a Light Blue app or another Curiosity board. BLE Advertising is broadcasting small packets to peer devices. In BLE, a peripheral device always starts with advertisements. Advertisement packets enable a central or observer to discover and connect to a peripheral.
Users can either choose to run the precompiled application example .hex file
on the Curiosity board and experience the demo or can go through the steps involved in
developing this application from scratch.
It is recommended to follow the examples in order, by learning the basic concepts first and then progressing to the more advanced topics.
Recommended Reading
- BLE Software Specification
- Getting Started with WME Bluetooth Low Energy Applications
Hardware Required
| Tool | Qty |
|---|---|
| Curiosity Board | 1 |
| Micro USB cable | 1 |
| Android/iOS Smartphone | 1 |
Software Requirement
- MPLAB X IPE: For programming the precompiled hex file.
- MPLAB X IDE: For programming the application example.
- Teraterm: Terminal Emulator for displaying UART output.
Programming the Precompiled Hex File or Application Example
Programming the .hex File using MPLAB X IPE
- Precompiled
.hexfiles are located in “<Harmony Content Path>wireless_apps_ble\apps\peripheral_conn\hex\“ folder. - For more information on the programming
steps, refer to the Programming a Device in MPLAB IPE.Note: Users must choose the correct device and tool information.
Programming the Application using MPLAB X IDE
- Follow the steps mentioned in Running a Precompiled Example
- Open and program the application example
“
peripheral_conn_xxxx.X” where xxxx refer to device (for example: WBZ451, project file:peripheral_conn_wbz451.X) located in “<Harmony Content Path>\wireless_apps_ble\apps\peripheral_conn\firmware” using MPLAB X IDE .
For more details on finding the Harmony content path, refer to Installing the MCC Plugin.
Demonstration
Developing the Application from Scratch using MCC
- Create a new MCC Harmony Project by selecting the device. For more details, refer to Creating a New MCC Harmony Project.
- Launch the MCC from the toolbar as
illustrated below. The project graph will open with the default components.
Figure 3-67. MCC - In the Device Resources window, expand
Libraries > Harmony > Wireless > Application Services. Then,
click the Plus Symbol to add the BLE Config App Service Component to the
project
Figure 3-68. BLE Config App Service - All BLE Stack related components will be added into the project graph. Accept dependencies or satisfiers by selecting Yes.
- For configuring BLE Config App Service component based on the device refer to Adding BLE Config App Service Component to Project Graph and Selecting the Device in Getting Started with WME Bluetooth Low Energy Applications from Related Links.
- To enable digital and communication interfaces, refer to Enabling Digital Input/Output and Communication Interfaces Through System Hardware Definition (SHD) component in Getting Started with WME Bluetooth Low Energy Applications from Related Links.
- For FreeRTOS component settings refer to the Configuring FreeRTOS in Getting Started with WME Bluetooth Low Energy Applications from Related Links.
- For WBZ451
- Verify if the project graph window
has all the expected components, as illustrated in the following figure:
Figure 3-69 3-71. Project Graph
- Verify if the project graph window
has all the expected components, as illustrated in the following figure:
- For WBZ351
- Change FreeRTOS Component
setting as illustrated in the following figure
Figure 3-70. FreeRTOS Component - Verify if the project graph window
has all the expected components. as illustrated in the following figure:
Figure 3-69 3-71. Project Graph
- Change FreeRTOS Component
setting as illustrated in the following figure
- Change BLE Stack Component
configuration as illustrated in the following figure.
Figure 3-72. BLE Stack Figure 3-73. BLE Stack
Generating a Code
For more details on code generation, refer to the MPLAB Code Configurator (MCC) Code Generation.
Files Containing User Application Code
| Source Files | Usage |
|---|---|
app.c | Application State machine, includes calls for Initialization of all BLE stack (GAP,GATT, SMP, L2CAP) related component configurations |
app_ble_callbacks.c | All the event functions related to GAP, GATT, SMP and L2CAP events that user can use or modify . |
app_utility.c | Contains generic utility functions that serve the purpose of providing reusable, common functionalities that can be applied across various parts of a program. |
app.c is auto generated and has a state
machine based application code sample. Users can use this template to develop their
application. Main application logic is implemented in void APP_Tasks() function.app.capp.c