3.10 Bluetooth® Low Energy Transparent UART Peripheral with LE Coded PHY
This section assists users in creating a peripheral device and sending/receiving characters between two connected BLE devices over the Microchip proprietary Transparent UART Profile with LE Coded PHY. The peripheral device will be a Curiosity board, and the central device will be another Curiosity board.
User can either choose to just run the precompiled application example
.hex files on the Curiosity board and experience the demo or can go
through the steps involved in developing this application from scratch.
These examples are incrementally structured upon one another. Recommendation is to follow the examples in order, by learning the basic concepts first and then progressing to the more advanced topics.
Recommended Reading
- BLE Software Specification
- Getting Started with WME Bluetooth Low Energy Applications
Hardware Requirement
| Tool | Quantity |
|---|---|
| Curiosity Board | 2 |
| Micro USB cable | 2 |
Software Requirement
- MPLAB X IPE: For programming the precompiled hex file.
- MPLAB X IDE: For programming the application example.
- Teraterm: Terminal Emulator for displaying UART output.
Programming the Precompiled Hex file or Application Example
Programming the .hex File using MPLAB X IPE
- Precompiled
.hexfile for peripheral is located in “<Harmony Content Path>\apps\peripheral_trp_uart_codedPhy\hex“ folder. - Precompiled
.hexfile for central is located in “<Harmony Content Path>\apps\central_trp_uart_codedPhy\hex“ folder. - For more information on the
programming steps, refer to the Programming a Device in MPLAB IPE.Note: Users must choose the correct device and tool information.
Programming the Application using MPLAB X IDE
- Follow the steps mentioned in Running a Precompiled Example
- Open and program the
peripheral application example
“
peripheral_trp_uart_codedPhy_xxxx.X” where xxxx refer to device (for example: WBZ451, project file:peripheral_trp_uart_codedPhy_wbz451.X) located in “<Harmony Content Path>\apps\peripheral_trp_uart_codedPhy\firmware” using MPLAB X IDE. - Open and program the central
application example “
central_trp_uart_codedPhy_xxxx.X” where xxxx refer to device (for example: WBZ451, project file:central_trp_uart_codedPhy_wbz451.X) located in “<Harmony Content Path>\apps\central_trp_uart_codedPhy\firmware” using MPLAB X IDE.
For more details on finding the Harmony content path, refer to Installing the MCC Plugin.
Demo Description
Developing the Application from Scratch using MCC
- Create a new MCC Harmony Project by selecting the device. For more details, refer to Creating a New MCC Harmony Project.
- Launch the MCC from the toolbar
as illustrated below. The project graph will open with the default
components.
Figure 3-108. MCC - In the Device Resources window,
expand Libraries > Harmony > Wireless > Application
Services. Then, click the Plus Symbol to add the
Transparent App Service Component to the project
Figure 3-109. Transparent App Service - All BLE Transparent App Service-related components will be added into the project graph. Accept dependencies or satisfiers by selecting Yes.
- For configuring BLE Config App Service component based on the device refer to Adding BLE Config App Service Component to Project Graph and Selecting the Device in Getting Started with WME Bluetooth Low Energy Applications from Related Links.
- To enable digital and communication interfaces, refer to Enabling Digital Input/Output and Communication Interfaces Through System Hardware Definition (SHD) component in Getting Started with WME Bluetooth Low Energy Applications from Related Links.
- Change the Transparent App
Service component settings as illustrated in the following figure.
Figure 3-110. Transparent App Service - Change FreeRTOS component
settings, refer to the Configuring FreeRTOS in Getting Started with
WME Bluetooth Low Energy Applications from Related Links.. Additionally,
change FreeRTOS component settings as illustrated in the following
figure.
- For WBZ451 FreeRTOS component setting
is as illustrated in the following figure
Figure 3-111. FreeRTOS - For WBZ351 FreeRTOS component setting
is as illustrated in the following figure
Figure 3-112. FreeRTOS
- For WBZ451 FreeRTOS component setting
is as illustrated in the following figure
- For WBZ451
- Verify if the project
graph window has all the expected components, as illustrated in the
following figure:
Figure 3-113. Project Graph
- Verify if the project
graph window has all the expected components, as illustrated in the
following figure:
- For WBZ351
- Verify if the project
graph window has all the expected components, as illustrated in the
following figure:
Figure 3-114. Project Graph
- Verify if the project
graph window has all the expected components, as illustrated in the
following figure:
- Change BLE Stack component
setting, as illustrated in the following figure:
Figure 3-115. BLE Stack Figure 3-116. BLE Stack
Generating a Code
For more details on code generation, refer to the MPLAB Code Configurator (MCC) Code Generation.
Files Containing User Application Code
| Source Files | Usage |
|---|---|
app.c | Application State machine, includes calls for Initialization of all BLE stack (GAP,GATT, SMP, L2CAP) related component configurations |
app_ble_callbacks.c | All the event functions related to GAP, GATT, SMP and L2CAP events that user can use or modify. |
app_trspc_callbacks.c | All the event functions related to
trspc event handles that user can use or
modify. |
app_utility.c | Contains generic utility functions that serve the purpose of providing reusable, common functionalities that can be applied across various parts of a program. |
app.c is auto generated and has
a state machine based application code sample. Users can use this template to
develop their application. Main application logic is implemented in void
APP_Tasks() function.app.capp.c