3.15 Bluetooth® Low Energy Proximity Monitor
This section guides users on configuration, programming, and validation of a BLE Proximity Monitor utilizing the Curiosity board, and also outlines the necessary hardware and software requirements, the BLE Proximity profile, and specific services involved. Additionally, it also includes step-by-step instructions and test cases to facilitate the implementation and verification of the application.
Recommended Reading
- BLE Software Specification
- Getting Started with WME Bluetooth Low Energy Applications
Hardware Requirement
|
Tool |
Quantity |
|---|---|
| Curiosity Board |
2 |
|
Micro USB Cable |
2 |
|
Laptop |
1 |
Software Requirements
- MPLAB X IPE: For programming the precompiled hex file.
- MPLAB X IDE: For programming the application example.
Programming the Precompiled Hex File or Application Example
Programming the .hex File using MPLAB X IPE
- Precompiled
.hexfile is located in “<Harmony Content Path>\wireless_apps_ble\apps\ble_pxpm_app\hex” folder. - For more information on the
programming steps, refer to the Programming a Device in MPLAB IPE.Note: Users must choose the correct device and tool information.
Programming the Application using MPLAB X IDE
- Follow the steps mentioned in Running a Precompiled Example
- Open and program the application
example “
ble_pxpm_app_xxxx.X” where xxxx refer to device (for example: WBZ451, project file: ble_pxpm_app_wbz451.X) located in “<Harmony Content Path>\wireless_apps_ble\apps\ble_pxpm_app\firmware” using MPLAB X IDE
For more details on finding the Harmony content path, refer to Installing the MCC Plugin.
Demo Description
- For WBZ451 refer: BLE Proximity Monitor
- For WBZ351 refer: BLE Proximity Monitor
Developing the Application from Scratch using MCC
- Create a new MCC Harmony Project by selecting the device. For more details, refer to Creating a New MCC Harmony Project.
- Launch the MPLAB Code
Configurator from the toolbar as illustrated below. The project graph will open
with the default components.
Figure 3-187. MCC - In the Device Resources window, expand Libraries > Harmony >
Wireless > Application Services. Then, click the Plus
Symbol to add the Proximity App Service Component to the project graph.
Figure 3-188. Proximity App Service - All BLE PXPM related components will be added into the project graph. Accept dependencies or satisfiers by selecting Yes.
- For configuring BLE Config App Service component based on the device refer to Adding BLE Config App Service Component to Project Graph and Selecting the Device in Getting Started with WME Bluetooth Low Energy Applications from Related Links.
- To enable digital and communication interfaces, refer to Enabling Digital Input/Output and Communication Interfaces Through System Hardware Definition (SHD) component in Getting Started with WME Bluetooth Low Energy Applications from Related Links.
- Change FreeRTOS component
settings as illustrated in the following figure. For more details, refer to the
Configuring FreeRTOS in Getting Started with WME Bluetooth Low
Energy Applications from Related Links.
Figure 3-189. FreeRTOS Configuration -
Select the Proximity App Service Component. In the Configuration Options, select the Enable Monitor Role. Additionally, ensure that the Support Immediate Alert Service, Support TX Power Service and Enable App Code Generation option is enabled.
Figure 3-190. Proximity App Service Configuration - For WBZ451
- Change
WBZ451-CURIOSITY Component setting as illustrated in the
following figure.
Figure 3-191. WBZ451-CURIOSITY Configuration - Verify if the project
graph window has all the expected components, as illustrated in the
following figure:
Figure 3-192. Project Graph
- Change
WBZ451-CURIOSITY Component setting as illustrated in the
following figure.
- For WBZ351
- Change
WBZ351-CURIOSITY Component setting as illustrated in the
following figure.
Figure 3-193. WBZ351-CURIOSITY Configuration - Verify if the project
graph window has all the expected components, as illustrated in the
following figure:
Figure 3-194. Project Graph
- Change
WBZ351-CURIOSITY Component setting as illustrated in the
following figure.
- Enabling the Enable Monitor
Role option in Proximity App Service component will configure
BLE Stack component . Additionally, selecting the Enable App Code
Generation option will generate the necessary application files related
to the service during the code generation process. Verify the BLE Stack
configuration.
Figure 3-195. BLE Stack Configuration Figure 3-196. BLE Stack Configuration
Generating a Code
For more details on code generation, refer to the MPLAB Code Configurator (MCC) Code Generation.
Files Containing User Application Code
| Source Files | Usage |
|---|---|
app.c | Application State machine, includes calls for Initialization of all BLE stack (GAP,GATT, SMP, L2CAP) related component configurations |
app_ble_callbacks.c | All the event functions related to GAP, GATT, SMP and L2CAP events that user can use or modify . |
app_pxpm_callbacks.c | All the event functions related to PXPM event handles that user can use or modify. |
app_utility.c | Contains generic utility functions that serve the purpose of providing reusable, common functionalities that can be applied across various parts of a program. |
app.c is auto generated and has
a state machine based application code sample. Users can use this template to
develop their application. Main application logic is implemented in void
APP_Tasks() function.app.capp.cProximity Profile
In the context of Bluetooth Low Energy, “proximity” generally refers to the physical closeness between two BLE devices. The BLE Proximity profile is a standardized BLE profile that enables a device to alert a user when another device is near or far away from it.
The Proximity profile defines the behavior when a device moves beyond the range of a peer device, resulting in either a disconnection or an increase in path loss exceeding the preset level, causing an immediate alert. This alert is used to notify the user that the devices has disconnected. As a consequence of this alert, a device may take further action.
- Proximity Reporter (Server): This refers to the tracked device, which could be an item like a key fob or any other asset whose proximity is to be monitored
- Proximity Monitor (Client): This device monitors the reporter's proximity, typically through a smart phone or tablet
The Proximity profile uses the Received Signal Strength Indicator (RSSI) to determine the approximate distance between the Monitor and the Reporter.
Role/Service Relationships
Proximity Monitor Requirements
The Proximity Monitor is designed to observe, connect, read, and configure a Proximity Reporter. Following are the detailed requirements and procedures for effective operation:
Service Discovery
The Proximity Monitor must perform service discovery to identify and connect to the following services by their respective UUIDs:
- Link Loss Service: Identified by the “Link Loss” service UUID.
- Immediate Alert Service: Identified by the “Immediate Alert” service UUID.
- TX Power Service: Identified by the “TX Power” service UUID.
- Discovery and
Configuration:
- Upon discovering the Link Loss Service and its alert level characteristic, the Proximity Monitor will write the alert level characteristic to the required link loss alert level. This action is performed once the connection between the Proximity Monitor and the Proximity Reporter is established.
- The required alert level can be set by the user of the Proximity Monitor.
- Connection
Monitoring:
- The Proximity Monitor can maintain an active connection with the Proximity Reporter and continuously monitor the RSSI of this connection.
- If the connection is disconnected, the Proximity Reporter will alert at the level specified in the alert level characteristic, as defined by the Link Loss Service specification.
- Discovery and
Reading:
- Upon discovering the Immediate Alert and TX Power Services, the Proximity Monitor can read the TX power level characteristic of the TX power service.
- This action is performed once the connection between the Proximity Monitor and the Proximity Reporter is established.
- Connection and Path Loss
Monitoring:
- The Proximity Monitor can maintain an active connection with the Proximity Reporter and continuously monitor the RSSI of this connection.
- The Proximity Monitor can calculate the path loss by subtracting the RSSI from the transmit power level of the Proximity Reporter, as determined by reading TX power procedure.
- If the path loss exceeds a threshold set on the Proximity Monitor, it can write to the alert level characteristic of the Immediate Alert Service using the GATT Write without Response sub-procedure. This action will cause the Proximity Reporter to alert.
Summary
The Proximity Monitor ensures continuous monitoring and configuration of the Proximity Reporter by:
- Discovering essential services and characteristics.
- Writing and setting alert levels as required.
- Monitoring the connection status and RSSI.
- Calculating path loss and triggering alerts based on predefined thresholds.
These procedures ensure that the Proximity Monitor effectively manages the Proximity Reporter, providing timely alerts and maintaining robust connectivity.
Proximity Monitor Application
In this section, the focus is on the Proximity Monitor application implementation specific details. In terms of the application design and testing methods
Working Flow
APP_PXP_IND_STA_IDLE: application remains in the Idle mode.APP_PXP_IND_STA_CONNECTED: application is prepared to transmit commands to the Proximity Reporter role.APP_PXP_IND_STA_WITH_BOND_SCAN: application is prepared to reconnect with bond withintimeout_with_bond_scanseconds duration.APP_PXP_IND_STA_SCAN: application is prepared to initiate the connection withintimeout_scanseconds duration.
Input and Output Interface
Input
The application relies on Button 1 as the input.
- Types of Pressing:
- Press: Pressing the button for less than 500 ms.
- Long press: Pressing the button for more than 500 ms.
- Application behavior on button press in different state co relation.
| State | Action | Behavior |
|---|---|---|
|
|
Long press Button 1 |
Connect to a new device |
|
|
Long press Button 1 |
Disconnect the existing connection and connect to a new device if available |
|
|
Long press Button 1 |
Start a new pairing |
On board RGB LED (for Alert Level) is used for the visual output information to the user.
Output
Immediate Alert level will be issued according to the following table.
|
Distance |
10 cm |
3m |
30m |
|---|---|---|---|
|
Path loss |
51 |
65 |
85 |
|
Zone |
LOW_ZONE |
MIDDLE_ZONE |
HIGH_ZONE |
|
APP Alert Level |
PXPM RGB LED Behavior | PXPR User LED |
|---|---|---|
|
|
Green Light | All LED keep lighting |
|
|
Red Light | User LED blinks one time every second |
|
|
OFF | User LED blinks five times every second |