3.2 Bluetooth® Low Energy Legacy Scan
This section guides users in enabling Bluetooth Low Energy Scanning on the Curiosity board using MCC. BLE scanning detects devices in Advertising Mode. Within BLE protocols, either a Central Device or an Observer initiates the scanning process.
Users can either run the precompiled application example .hex file on
the Curiosity Board to experience the demo or follow the steps to develop this
application from scratch.
It is recommended to follow the examples in order, starting with the basic concepts and then progressing to more advanced topics.
Recommended Reading
- BLE Software Specification
- Getting Started with WME Bluetooth Low Energy Applications
Hardware Requirement
| Tool | Qty |
|---|---|
| Curiosity Board | 1 |
| Micro USB cable | 1 |
Software
- MPLAB X IPE: For programming the precompiled hex file.
- MPLAB X IDE: For programming the application example.
- Teraterm: Terminal Emulator for displaying UART output.
Programming the Precompiled
.hex File or Application Example
Programming the .hex file using MPLAB X IPE
-
Precompiled
.hexfile is located in the path“<Harmony Content Path>\wireless_apps_ble\apps\legacy_scan\hex”folder - For more information on the
programming steps, refer to the Programming a Device in MPLAB IPE.Note: Users must choose the correct device and tool information.
Programming the Application using MPLAB X IDE
- Follow the steps mentioned in Running a Precompiled Example
-
Open and program the application example “
legacy_scan_xxxx.X” where xxxx refer to device ( for example: WBZ451, project file:legacy_scan_wbz451.X) located in “<Harmony Content Path>\wirelss_apps_ble\apps\legacy_scan\firmware” using MPLAB X IDE
For more details on finding the Harmony content path, refer to Installing the MCC Plugin.
Demo Description
Developing this Application from Scratch Using MCC
- Create a new MCC Harmony Project by selecting the device. For more details, refer to Creating a New MCC Harmony Project.
- Launch the MCC from the toolbar as
illustrated below. The project graph will open with the default components.
Figure 3-31. MCC - In the Device Resources window,
expand Libraries > Harmony > Wireless > Application Services.
Then, click the Plus Symbol to add the BLE Config App Service
Component to the project
Figure 3-32. BLE Config App Service - All BLE Stack related components will be added into the project graph. Please accept dependencies or satisfiers by selecting Yes.
- To enable digital and communication interfaces, refer to Enabling Digital Input/Output and Communication Interfaces Through System Hardware Definition (SHD) component in Getting Started with WME Bluetooth Low Energy Applications from Related Links.
- For configuring BLE Config App Service component based on the device refer to Adding BLE Config App Service Component to Project Graph and Selecting the Device in Getting Started with WME Bluetooth Low Energy Applications from Related Links.
- For FreeRTOS component settings refer to the Configuring FreeRTOS in Getting Started with WME Bluetooth Low Energy Applications from Related Links.
- For WBZ451
- Verify if the project graph
window has all the expected components, as illustrated in the following
figure:
Figure 3-33. Project Graph
- Verify if the project graph
window has all the expected components, as illustrated in the following
figure:
- For WBZ351
- Verify if the project graph
window has all the expected components, as illustrated in the following
figure:
Figure 3-34. Project Graph
- Verify if the project graph
window has all the expected components, as illustrated in the following
figure:
- Change the BLE Stack Component
settings as illustrated in the following figure
Figure 3-35. BLE Stack
Generating a Code
For more details on code generation, refer to the MPLAB Code Configurator (MCC) Code Generation.
Files Containing User Application Code
Details on files that user can modify
| Source Files | Usage |
|---|---|
app.c | Application State machine, includes calls for Initialization of all BLE stack (GAP,GATT, SMP, L2CAP) related component configurations |
app_ble_callbacks.c | All the event functions related to GAP, GATT, SMP and L2CAP events that user can use or modify . |
app_utility.c | Contains generic utility functions that serve the purpose of providing reusable, common functionalities that can be applied across various parts of a program. |
app.c is auto generated and has a state
machine based application code sample. Users can use this template to develop their
application. Main application logic is implemented in void
APP_Tasks() function.app.c