1.26.6.28 MCANx_RxBuffersCallbackRegister Function
C
void MCANx_RxBuffersCallbackRegister(MCAN_TXRX_BUFFERS_CALLBACK callback, uintptr_t contextHandle) // x - Instance of the MCAN peripheral
Summary
Sets the pointer to the function (and it's contextHandle) to be called when the given MCAN's Rx transfer events occur.
Precondition
MCANx_Initialize must have been called for the associated MCAN instance.
Parameters
Param | Description |
---|---|
callback | A pointer to callback function which function prototype definedby the MCAN_TXRX_BUFFERS_CALLBACK data type. |
contextHandle | A value passed into the callback function as callback parameter. |
Returns
None.
Example
void APP_MCAN_RxBufferCallback(uint8_t bufferNumber, uintptr_t context)
{
}
MCAN0_RxBuffersCallbackRegister(APP_MCAN_RxBufferCallback, NULL);
Remarks
None.