2.122.4 TIMER32_x_PreLoadCountSet Function
C
/* x = Timer32 instance number */
void TIMER32_x_PreLoadCountSet(uint32_t count)
Summary
Sets the timer pre-load value
Description
Sets the timer pre-load value. This is used by H/W when the counter is to be restarted automatically; this will become the new value of the counter upon restart.
Precondition
TIMER32_x_Initialize() function must have been called first and auto-restart must be enabled
Parameters
| Param | Description |
|---|---|
| count | timer pre-load value |
Returns
None
Example
TIMER32_0_PreLoadCountSet(1000);
Remarks
None