2.39.7 ECIA_GIRQResultGet Function
C
uint8_t ECIA_GIRQResultGet(ECIA_INT_SOURCE int_src)
Summary
Returns the status of the given interrupt source
Description
Returns the status of the given interrupt source. The status is returned as 1 if both the interrupt source is active and the corresponding interrupt is enabled. The status is returned as 0 otherwise.
Precondition
None.
Parameters
| Param | Description |
|---|---|
| int_src | One of the interrupt source from the enum ECIA_INT_SOURCE |
Returns
1 - Interrupt source is active and interrupt is enabled
0 - Interrupt source is not active or interrupt is disabled
Example
uint8_t result = ECIA_GIRQResultGet(ECIA_AGG_INT_SRC_GPIO002)
Remarks
None