2.39.5 ECIA_GIRQBlockStatusGet Function
C
uint32_t ECIA_GIRQBlockStatusGet(ECIA_GIRQ_BLOCK_NUM block)
Summary
Reports the status of the group GIRQ interrupt assertion to the NVIC.
Description
Reports the status of the group GIRQ interrupt assertion to the NVIC.
Precondition
None.
Parameters
| Param | Description |
|---|---|
| block | One of the GIRQ block number from the enum ECIA_GIRQ_BLOCK_NUM |
Returns
None
Example
uint32_t status = ECIA_GIRQBlockStatusGet(ECIA_GIRQ_BLOCK_NUM8);
Remarks
None