2.87.3 POWER_WakeupSourceGet Function
C
POWER_WAKEUP_SOURCE POWER_WakeupSourceGet( void );
Summary
Returns the source of wakeup from deep sleep
Description
This function returns the name of the source which woke up the device from deep sleep.
Precondition
None.
Parameters
None.
Returns
POWER_WAKEUP_SOURCE - wakeup source
Example
if (POWER_WakeupSourceGet() == POWER_WAKEUP_SOURCE_DSINT0)
{
// wakeup source was INT0
}
Remarks
This function is only available for the devices which has deep sleep controller. MCC will generate this function only for the selected devices accordingly. Check device datasheet for more information.