2.104.1 SDADC_Initialize Function
C
void SDADC_Initialize( void )
Summary
Initializes given instance of SDADC peripheral.
Description
This function initializes given instance of SDADC peripheral of the device with the values configured in MCC GUI. Once the peripheral is initialized, peripheral can be used for conversion.
Precondition
MCC GUI should be configured with the right values.
Parameters
None.
Returns
None.
Example
SDADC_Initialize();
Remarks
This function must be called before any other SDADC function is called. This function should only be called once during system initialization.