2.104.8 SDADC_WindowMonitorIsSet Function
C
bool SDADC_WindowMonitorIsSet( void )
Summary
Returns the status of the window monitor.
Description
This function returns the status of whether window monitor condition is met.
Precondition
SDADC_Initialize() function must have been called first for the associated instance. Also conversion must have been started.
Parameters
None.
Returns
true - Window monitor condition is met false - Window monitor condition is not met
Example
bool sdadcWinMonStatus; SDADC_Initialize(); SDADC_ConversionStart(); sdadcWinMonStatus = SDADC_WindowMonitorIsSet();
Remarks
This function should be called only after conversion is started and window monitor mode is enabled.