2.129.6 TWIHSx_ErrorGet Function
C
/* x = TWIHS instance number */
/* TWIHS master mode */
TWIHS_ERROR TWIHSx_ErrorGet(void)
Summary
Returns the TWIHS error that occurred on the bus.
Description
This function returns the TWIHS error that occurred on the bus. The function can be called to identify the error cause.
Precondition
TWIHSx_Initialize must have been called for the associated TWIHS instance.
Parameters
None.
Returns
Returns error of type TWIHS_ERROR, identifying the error that has occurred.
Example
if(TWIHS1_ErrorGet() == TWIHS_ERROR_NONE)
{
//Transfer is completed successfully
}
else
{
//Error occurred during transfer.
}
Remarks
None