2.120.1.14 TCx_Timer8bitCompareSet Function
C
/* x = TC instance number */ void TCx_Timer8bitCompareSet ( uint8_t compare );
Summary
Sets the compare value of a given timer channel.
Description
This function writes the compare value. When timer counter matches compare value, interrupt can be generated.
Precondition
TCx_TimerInitialize function must have been called first for the given channel.
Parameters
| Param | Description |
|---|---|
| compare | compare value of the timer |
Returns
None.
Example
TC0_TimerInitialize();
TC0_Timer8bitCompareSet(0xFul);
Remarks
This function is available only when TC timer mode is used by SYS_TIME module. SYS_TIME uses compare match interrupt to generate dynamic delay.