4.1.2 Interrupt and Trap Vectors
All dsPIC33CK1024MP710 family
devices reserve addresses between 0x000000 and 0x000200 for hard-coded program execution
vectors. A hardware Reset vector is provided to redirect code execution from the default
value of the PC on device Reset to the actual start of code. A GOTO
instruction is programmed by the user application at address 0x000000 of Flash memory,
with the actual address for the start of code at address 0x000002 of Flash memory.
A more detailed discussion of the Interrupt Vector Tables (IVTs) is provided in Interrupt Controller.