7.1 Interrupt Vector Table
The dsPIC33CK1024MP710 family Interrupt Vector Table (IVT), shown in Figure 7-1, resides in program memory, starting at location, 0x000004. The IVT contains six non-maskable trap vectors and up to 246 sources of interrupts. In general, each interrupt source has its own vector. Each interrupt vector contains a 24-bit wide address. The value programmed into each interrupt vector location is the starting address of the associated Interrupt Service Routine (ISR).
- In Dual Partition modes, each partition has a dedicated Interrupt Vector Table.
- See Trap Vector Details.
Interrupt vectors are prioritized in terms of their natural priority. This priority is linked to their position in the vector table. Lower addresses generally have a higher natural priority. For example, the interrupt associated with Vector 0 takes priority over interrupts at any other vector address.