2.1 Basic Connection Requirements
Getting started with the family devices of the dsPIC33CK1024MP710 requires attention to a minimal set of device pin connections before proceeding with development. The following is a list of pin names which must always be connected:
- All VDD and VSS pins (see Decoupling Capacitors)
- All AVDD and AVSS pins regardless if ADC module is not used (see Decoupling Capacitors)
- MCLR pin (see Master Clear (MCLR) Pin)
- PGCx/PGDx pins used for In-Circuit Serial Programming™ (ICSP™) and debugging purposes (see ICSP Pins)
- OSCI and OSCO pins when an external oscillator source is used (see External Oscillator Pins)