12.5 PWM Control/Status Registers

There are two categories of Special Function Registers (SFRs) used to control the operation of the PWM module:

  • Common, shared by all PWM Generators
  • PWM Generator-specific
  • Auxiliary PWM which is used as additional PWM Generators

An ‘x’ in the register name denotes an instance of a PWM Generator.

A ‘y’ in the register name denotes an instance of the common function.

An ‘A’ in the register name denotes an instance of the Auxiliary PWM.