5.7.8.6 Include Option
The -include file
option processes
file
as if #include "file"
appeared as
the first line of the primary source file. In effect, the contents of
file
are compiled first. Any -D
and
-U
options on the command line are always processed before the
-include
option, regardless of the order in which they are written.
All the -include
and -imacros
options are processed in
the order in which they are written.