4.7.1.1.8 Tips and Tricks
The following information could be helpful when using the Dashboard:
- When colors are default or cleared,
most widgets will adapt to the light or dark theme selection
. If
colors are set, then the theme will not affect the colors. However, it is always
possible to change or clear colors. - When resizing a widget with text, the
text may overflow the bounds of the widget. There is a "text wrapping" setting for
the text widgets that changes how the text overflows. Nevertheless, the text will
overflow if the widget is too small.
To prevent text overflow, clear the width and height property of the widget (the 'x' on the right of those properties in the options.) The text widget will then size to adapt to the content.