2.10 Programming the Device on the Evaluation Board
(Ask a Question)After generating the bitstream, the PolarFire device must be programmed with the Auto Update and IAP design.
To program the PolarFire device, perform the following steps:
- Ensure that the following jumper
settings are set on the board.
Table 2-3. Jumper Settings—Evaluation Board Jumper Description J18, J19, J20, J21, and J22 Close pin 2 and 3 for programming the PolarFire FPGA through FTDI J28 Close pin 1 and 2 for programming through the on-board FlashPro5 J23 Open pin 1 and 2 for accessing external SPI Flash J4 Close pin 1 and 2 for manual power switching using SW3 J12 Close pin 3 and 4 for 2.5 V - Connect the power supply cable to the J9 connector on the board.
- Connect the USB cable from the host PC to the J5 (FTDI port) on the board.
- Power ON the board using the SW3
slide switch.
The following figure shows the board setup after these connections are made.
Figure 2-12. Board Setup—Evaluation Kit - On the Libero Design Flow, double-click Run PROGRAM Action.
The device is successfully programmed and the on-board LEDs glow. A green tick mark appears next to Run PROGRAM Action, see Figure 2-2.