22.4.2 Setup for PWM Operation
Take these steps when configuring the CCP module for standard PWM operation:
- Use the desired output pin RxyPPS control to select CCPx as the source and disable the CCPx pin output driver by setting the associated TRIS bit.
- Load the T2PR register with the PWM period value.
- Configure the CCP module for the PWM mode by loading the CCPxCON register with the appropriate values.
- Load the CCPRx register with the PWM duty cycle value and configure the FMT bit to set the proper register alignment.
- Configure and start Timer2:- Clear the TMR2IF interrupt flag bit of the PIR4 register. See the Note below.
- Select the timer clock source to be FOSC/4 using the TxCLKCON register. This is required for correct operation of the PWM module.
- Configure the T2CKPS bits of the T2CON register with the timer prescale value
- Enable the timer by setting the T2ON bit
 
- Enable the PWM output pin:- Wait until the timer overflows and the TMR2IF bit of the PIR4 register is set. See the Note below.
- Enable the CCPx pin output driver by clearing the
                  associated TRIS bitImportant: To send a complete duty cycle and period on the first PWM output, the above steps must be included in the setup sequence. If it is not critical to start with a complete PWM signal on the first output, then step 6 may be ignored.