23.2 Document Conventions
This document uses the following variables:
- FPGA family libraries are shown as
<act_fam>. Substitute the desired FPGA family variable with the device family
as needed. For example:
vcom -work <vhd_fam> <act_fam>.vhd
- Compiled VHDL libraries are shown as
<vhd_fam>. Substitute<vhd_fam>for the desired VHDL family variable as needed. The VHDL language requires that the library names begin with an alpha character.