13.19.3.2 Adding/Renaming Ports

To add ports:

  1. From the SmartDesign menu, choose Logic > Add port. The Add Port dialog box appears (as shown below).
    Figure 13-53. Add New Port Dialog Box
    ???
  2. Specify the name of the port you wish to add. You can specify a bus port by indicating the bus width directly into the name using brackets [ ], such as mybus[3:0].
  3. Select the direction of the port.

To remove a port from the top level, select the port in the Grid, right-click and choose Delete Top Level Port.

To rename a top-level port, right-click the top-level non-pad port and choose Modify Top Level Port. You can rename the port, change the bus width (if the port is a bus), and change the port direction.

To rename an external pad:

  1. Right-click a pad in the top-level port and select Rename External Pad. The Rename External Pad dialog box appears, as shown in the figure below.
    Figure 13-54. Rename External Pad Dialog Box
    ???
  2. Enter the new name for the external pad and click OK.