24.3 Document Conventions

This document uses the following conventions:

Information input by the user follows this format:

keyboard input

The contents of a file follows this format:

file contents

This document uses the following variables:

  • Microchip FPGA family libraries are shown as <act_fam>. Substitute the desired Microchip FPGA family variable with Fusion, IGLOOTM/e, ProASIC3/E, act1, act2 (for ACT2 and 1200XL devices), ACT3, 3200DX, MX, SX, SX-A, eX, Axcelerator, A500k, and APA as needed. For example:

    vlog -work <act_fam> <act_fam>.v