20.1.1.5 MCHP Flash Enable
(MCHP_FLASH_ENABLE) Instruction
MCHP_FLASH_ENABLE sets the FAEN bit, which controls processor access to
the Flash memory. The FAEN bit’s state is returned in the field of the same name. This
command has no effect if CPS = 0. This command requires a
NOP to complete.Note: This command is not
required for PIC32MZ and PIC32MK family devices.