6.1 Set Mode (SetMode) Pseudo
Operation
Format:
SetMode (mode)
Purpose:
- To set the EJTAG state machine to a specific state.
Description:
- The value of mode is clocked into the device on signal TMS. TDI is set to
‘
0’ and TDO is ignored.
Restrictions:
- None.
Example:
- The following is an example of how to use the
SetModefunction:SetMode (6’b011111)