6.3 Transfer Data (XferData)
Pseudo Operation
Format:
oData = XferData (iData)
Purpose:
- To clock data to and from the register selected by the command.
Description (in sequence):
- The TMS Header is clocked into the device to select the Shift DR state.
- The data is clocked in/out of the device on TDI/TDO while holding signal TMS low.
- The last MSb of the data is clocked in/out while setting TMS high.
- The TMS Footer is clocked in on TMS to return the TAP controller to the Run/Test Idle state.
Restrictions:
- None.
Example:
- The following is an example of how to use the Transfer Data
(
XferData) function:oData = XferData (32’h0x12)
XferData) Four-WireXferData) Two-Wire (4-phase)