2.1.4.3 DRV_MCMETROLOGY_Open Function
C
DRV_MCMETROLOGY_RESULT DRV_MCMETROLOGY_Open (
DRV_MCMETROLOGY_START_MODE mode,
DRV_MCMETROLOGY_CONTROL * pConfiguration
);
Summary
Opens the metrology driver according to the mode parameter.
Description
This routine enables the IPC peripheral and, only if a HARD Start mode has been selected, handles the reset and clock lines for enabling the metrology library application. On the other hand, SOFT mode does not any effects on metrology library application running in the second processor.
Parameters
| Parameters | Description |
|---|---|
| mode | Metrology Driver Start mode |
| pConfiguration | Pointer to CONTROL configuration to be loaded. In case of NULL, the MCC default configuration will be loaded |
Returns
If successful, returns DRV_MCMETROLOGY_SUCCESS. Otherwise, it returns DRV_MCMETROLOGY_ERROR.
Example
/* Detection of the WDOG0 Reset */
if (RSTC_ResetCauseGet() == RSTC_SR_RSTTYP(RSTC_SR_RSTTYP_WDT0_RST_Val))
{
app_metrologyData.startMode = DRV_MCMETROLOGY_START_SOFT;
}
else
{
app_metrologyData.startMode = DRV_MCMETROLOGY_START_HARD;
}
...
case APP_METROLOGY_STATE_INIT:
{
if (DRV_MCMETROLOGY_Open(app_metrologyData.startMode, NULL) == DRV_MCMETROLOGY_SUCCESS)
{
if (app_metrologyData.startMode == DRV_MCMETROLOGY_START_HARD)
{
app_metrologyData.state = APP_METROLOGY_STATE_START;
}
else
{
app_metrologyData.state = APP_METROLOGY_STATE_RUNNING;
}
}
else
{
app_metrologyData.state = APP_METROLOGY_STATE_ERROR;
}
break;
}
Remarks
This routine must be called after DRV_MCMETROLOGY_Initialize routine is called.