3.4.8.1 Obtain Customer UUID from Microchip
Customer UUID (U_UUID) is a 32-symbol hex string identifier that is assigned by Microchip through the Microchip portal (see the Secure Production Programming Solution (SPPS) User Guide for details).
Example of the customer UUID: 00000000000000000000000000000001.
Note: UUID must have all lower case characters.
Private/Public SEE keys must use the Customer UUID assigned by Microchip.
Once the UUID value is available, update the tag in both U-HSMMaster.config files, under the server and tools directories, as explained in section Update Server and Tools Configurations.