4.4.1 Paged Memory Scheme
The dsPIC33CK512MP608 architecture
extends the available Data Space through a paging scheme, which allows the available
Data Space to be accessed using MOV instructions in a linear fashion
for pre-modified and post-modified Effective Addresses (EAs). The upper half of the base
Data Space address is used in conjunction with the Data Space Read Page (DSRPAG)
register to form the Program Space Visibility (PSV) address.
The DSRPAG register is located in the SFR space. When DSRPAG[9] =
1 and the base address bit EA[15] = 1, the
DSRPAG[8:0] bits are concatenated onto EA[14:0] to form the 24-bit PSV read address.
The paged memory scheme provides access to multiple 32-Kbyte windows in the PSV memory. The DSRPAG register, in combination with the upper half of the Data Space address, can provide up to 8 Mbytes of PSV address space. The paged data memory space is shown in Figure 4-8.
The Program Space (PS) can be accessed with a DSRPAG of 0x200 or greater. Only reads from PS are supported using the DSRPAG.
When a PSV page overflow or underflow occurs, EA[15] is cleared as a result of the register indirect EA calculation. An overflow or underflow of the EA in the PSV pages can occur at the page boundaries when:
- The initial address, prior to modification, addresses the PSV page
- The EA calculation uses Pre-Modified or Post-Modified Register Indirect Addressing; however, this does not include Register Offset Addressing
In general, when an overflow is detected, the DSRPAG register is incremented and the EA[15] bit is set to keep the base address within the PSV window. When an underflow is detected, the DSRPAG register is decremented and the EA[15] bit is set to keep the base address within the PSV window. This creates a linear PSV address space, but only when using Register Indirect Addressing modes.
Exceptions to the operation described above arise when entering and exiting the boundaries of Page 0 and PSV spaces. Table 4-2 lists the effects of overflow and underflow scenarios at different boundaries.
In the following cases, when overflow or underflow occurs, the EA[15] bit is set and the DSRPAG is not modified; therefore, the EA will wrap to the beginning of the current page:
- Register Indirect with Register Offset Addressing
- Modulo Addressing
- Bit-Reversed Addressing
| O/U, R/W | Operation | Before | After | ||||
|---|---|---|---|---|---|---|---|
| DSRPAG | DS EA[15] | Page Description | DSRPAG | DS EA[15] | Page Description | ||
| O, Read | [++Wn]or
| DSRPAG = 0x2FF | 1 | PSV: Last lsw page | DSRPAG = 0x300 | 1 | PSV: First MSB page |
| O, Read | DSRPAG = 0x3FF | 1 | PSV: Last MSB page | DSRPAG = 0x3FF | 0 | See Note 1 | |
| U, Read | [--Wn]or
| DSRPAG = 0x001 | 1 | PSV page | DSRPAG = 0x001 | 0 | See Note 1 |
| U, Read | DSRPAG = 0x200 | 1 | PSV: First lsw page | DSRPAG = 0x200 | 0 | See Note 1 | |
| U, Read | DSRPAG = 0x300 | 1 | PSV: First MSB page | DSRPAG = 0x2FF | 1 | PSV: Last lsw page | |
| Legend: O = Overflow, U = Underflow, R = Read, W =
Write Note:
| |||||||