3.4.1 A: Listing Option
The -a[suboption]
[=file] option enables an assembler list file output and
controls what is included in the listing. The forms of this option and their meaning are
given in the following table.
-ac | Omit false conditionals |
-ad | Omit debugging directives |
-ah | Include high-level source |
-al | Include assembly |
-am
| Include macro expansions |
-an
| Omit forms processing |
-as | Include symbols |
-a=file | Output listing to specified file (must be in current directory). |
If no sub-options are specified, the default sub-options used are hls; the -a option by itself
requests high-level, assembly, and symbolic listing. You can use other letters to select
specific options for the listing output.
The letters after the -a may be combined into one option. So for example instead of specifying -al -an on the command line, you could specify -aln.