2.1.3.2 LSRAM Configurator
(Ask a Question)The Libero SoC software catalog has the following LSRAM configuration tools:
Using these configurators, the LSRAM can be configured as per design requirements. The generated LSRAM component can be instantiated in the SmartDesign. The configurators generate the HDL wrapper files for LSRAM with the appropriate values assigned to the static signals. Use the generated HDL wrapper files in the design hierarchy by connecting the ports to the rest of the design.