2.1.3.2.1 Dual-Port Large SRAM Configurator

The PF_DPSRAM configurator is available in the Libero SoC IP Catalog > Memory & Controllers.

The PF_DPSRAM configurator automatically cascades LSRAM blocks to create wider and deeper memories by selecting the most efficient aspect ratio. It also handles the grounding of unused bits. The configurator supports the generation of memories that have different aspect ratios on each port. The configurator uses one or more memory blocks to generate a RAM to match the configuration. The configurator also creates an external logic required for the cascading.

The configurator cascades RAM blocks in three different methods:

  • Cascaded deep—For example, two blocks of 16384 x 1 are combined to create a 32768 x 1.
  • Cascaded wide—For example, two blocks of 16384 x 1 are combined to create a 16384 x 2.
  • Cascaded wide and deep—For example, four blocks of 16384 x 1 are combined to create a 32768 x 2, in a two-block width by two-block depth configuration.

For more information on Dual-Port mode, see Dual-Port Mode.

Figure 2-12. Dual-Port Large SRAM Configurator: Generated Component
Table 2-9. Dual-Port LSRAM Configurator Signals
PortDirectionPolarityDescription
CLKInputRising edgeSingle-clock signal that drives both ports with the same clock. Exposed only when single clock is selected.
A_DIN[19:0]Input—Port A write data
A_ADDR[9:0]Input—Port A read address
A_BLK_ENInputActive HighPort A block select
A_CLKInputRising edgePort A clock. Applicable only when independent clocks are selected.
A_WENInput—Port A signal to switch between write and read modes:
  • Low: Read
  • High: Write
A_RENInput—Port A read data enable
A_WBYTE_EN[1:0]Input—Port A write byte enable
A_DOUT[19:0]Output—Port A read data
A_DOUT_ENInputActive HighPort A read data register enable
A_DOUT_SRST_NInputActive LowPort A read data register synchronous reset
A_DOUT_ARST_NInputActive LowPort A read data register asynchronous reset
B_DIN[19:0]Input—Port B write data
B_ADDR[9:0]Input—Port B address
B_BLK_ENInputActive HighPort B enable
B_CLKInputRising edgePort B clock. Applicable only when independent clocks are selected
B_WENInput—Port signal to switch between write and read modes:
  • Low: Read
  • High: Write
B_RENInput—Port B read data enable
B_WBYTE_EN[1:0]Input—Port B write byte enable
B_DOUT[19:0]Output—Port B read data
B_DOUT_ENInputActive HighPort B read data register enable
B_DOUT_SRST_NInputActive LowPort B read data register synchronous reset
B_DOUT_ARST_NInputActive LowPort B read data register asynchronous reset
ACCESS_BUSYOutputActive HighBusy signal when being initialized or accessed using SmartDebug

The dual-port LSRAM configurator has three tabs:

  • Parameter settings
  • Port settings
  • Memory initialization

Parameter Settings

The parameter settings include the optimization of LSRAM for High Speed or Low Power, clock signal settings, and optional port settings. The following figure shows the Dual-Port Large LSRAM block configurator.

Figure 2-13. Dual-Port Large SRAM Configurator: Parameter Settings

Optimization for High Speed or Low Power

You can optimize the LSRAM with one of the following options:
  • High Speed—Optimizes the LSRAM for speed and area by using width cascading.
  • Low Power—Optimizes the LSRAM for low power by using depth cascading, it uses additional logic at the input and output.

Single Clock (CLK) or Independent Clocks (A_CLK and B_CLK)

You can set the clock signals and the signal polarity:
  • Single clock—Drives both A and B ports with the same clock. This is the default configuration for dual-port LSRAM.
  • Independent clocks—Selects independent clock for each A_CLK for Port A and B_CLK for Port B).
  • Rising edge or Falling edge—Changes the signal polarity.

Optional Ports

You can select one of the following optional ports:
  • Lock access to SmartDebug—When enabled, SmartDebug access to the RAM is disabled.
  • Expose ACCESS_BUSY output—When enabled, SmartDebug ACCESS_BUSY signal is available as top-level port.

Port Settings

In the Port Settings tab, you can set the RAM size, select ports, and set data output on write settings for both Ports A and B. The following figure shows the PF_DPSRAM block port settings.

Figure 2-14. Dual-Port Large SRAM Configurator: Port Settings

Byte Enable Settings

Write Byte Enables—Enables writing to individual bytes of data (A_WBYTE_EN and B_WBYTE_EN).

The Write Byte Enable bits are all the control signals exposed by each column of LSRAM blocks when the implementation splits the word width. The LSRAM configurator generates the most efficient configuration of the depth and width for high-speed or low-power selection. Depending on the generated configuration, each Write Byte Enable bit may control up to 10 bits of data. In other words, the Write Byte Enable option does not govern the implementation.

In low-power mode for word widths that are multiples of 8, each Write Byte Enable bit controls 8 bits unless the word width is also a multiple of 10. For example, generating a 32-bit word width LSRAM, with Write Byte Enables, cascades the RAMs width-wise such that there are a total of 4 Write Byte Enable bits (2 per RAM block) and each Write Byte Enable bit controls the writing of 8-bits of data.

Other Examples are as follows:
  • Width of 17, is divided as 9 + 8.
  • Width of 35, is first divided as 18 + 17, and then, divided as 9 + 9 + 9 + 8.

RAM Size

You can set the RAM size.
  • Depth—Sets the depth range. The depth range for each port is between 1 and 524288. The maximum value depends on the die.
  • Width—Sets the width range. The width range for each port is between 1 and 19040.
Important: The two ports can be configured independently for any depth and width. However, Port A depth x Port A width must be equal to Port B depth x Port B width. The width range varies between devices.

Ports Selection: Block Select (A_BLK_EN and B_BLK_EN)

The default configuration for A_BLK_EN and B_BLK_EN is unchecked, which ties the signal to the Active state and removes it from the generated component. Select Active high or Active low to change the signal polarity. Ports are populated on the component by checking the respective check boxes.

Read Enable (A_REN and B_REN)

The default configuration for A_REN or B_REN is unchecked, which ties the signal to the active state and removes it from the generated macro. Select Active high or Active low to change the signal polarity. Ports are populated on the component by checking the respective check boxes.

Enable Pipeline

Check the Enable Pipeline check box to enable pipelining of read data (A_DOUT or B_DOUT). If the Enable Pipeline check box is disabled, you cannot configure the A_DOUT_EN/B_DOUT_EN, A_DOUT_SRST_N/B_DOUT_SRST_N, or A_DOUT_ARST_N/B_DOUT_ARST_N signals.
  • Register Enable (A_DOUT_EN and B_DOUT_EN)—the pipeline registers for ports A and B have active-high, enable inputs. By default, the check box is disabled. Selecting this check box adds the signal to the top-level port.
  • Synchronous Reset (A_DOUT_SRST_N and B_DOUT_SRST_N)—the pipeline registers for ports A and B have active-low, synchronous reset inputs. By default, the check box is disabled. Selecting this check box adds the signal to the top-level port.
  • Asynchronous Reset (A_DOUT_ARST_N and B_DOUT_ARST_N)—the pipeline registers for ports A and B have active-low, asynchronous reset inputs. By default, the check box is disabled. Selecting this check box adds the signal to the top-level port.

Select Active high or Active low to change the signal polarity. Ports are populated on the component by checking their respective check boxes.

Data Output on Write

Select the required option from the following:
  • Previous DOUT—The default data on the Read data output (A_DOUT or B_DOUT) during a write cycle is the DOUT data from the previous cycle (Previous DOUT).
  • DIN—To enable feed-through write mode on Read data output.
  • Read before Write—To perform a read operation before a write operation overwriting the previous data.

Memory Initialization at Power-Up

In the Memory Initialization tab, you can initialize RAM at power-up. LSRAM can be initialized during device power-up and functional simulation. The following figure shows the PF Dual Port Large SRAM IP memory initialization.

Figure 2-15. Dual-Port Large SRAM Configurator: Memory Initialization

Initialize RAM at Power Up

You can initialize RAM during power-up of the device by setting the following:
  • Initialize RAM at Power Up—Loads the RAM content during device operation at power-up and functional simulation.
  • RAM Configuration—Both write and read depths and widths are displayed as specified in the Port settings tab.
  • Initialize RAM Contents From File—The RAM’s content can be initialized by importing the memory file. This avoids the simulation cycles required for initializing the memory and reduces the simulation runtime. The configurator partitions the memory file appropriately so that the right content goes to the right block RAM when multiple blocks are cascaded.
  • Import File—Selects and imports a memory content file (Intel-Hex) from the Import Memory Content dialog box. File extensions are set to *.hex for Intel-Hex files during import. For more information, see Appendix: Supported Memory File Formats for LSRAM and μSRAM. The imported memory content is displayed in the RAM Content Editor.
  • Reset All Values—Resets all the data values. This option is enabled when the RAM Content Editor check box is selected.

RAM Content Editor

The RAM Content Editor enables the user to specify the contents of RAM memory manually for both Port A and Port B. It also allows you to modify imported data.

Port A View/Port B View
  • Go To Address—Enables you to go to a specific address in the editor. You can select the number display format (HEX, BIN, and DEC) from the Address menu.
  • Default Data Value—You can set this with new data to change the default. When the data value is changed, all default values in the manager are updated to match the new value. You can select the number display format (HEX, BIN, and DEC) from the Data menu.
  • Address—The Address column lists the address of a memory location. The menu specifies the number format of the address list (hexadecimal, binary, or decimal).
  • Data—Controls the data format and data values in the manager.

Click OK to close the manager and save all changes made to the memory and its contents. Click Cancel to close the manager and cancel all the changes.

Important: The dialogs show all data with the MSb down to LSb. For example, if the row showed 0xAABB for a 16-bit word size, the AA is MSb and BB is LSb.