3.10 UWB Device – Register Reset Values Change

The ATA8352 UWB device has a set of registers that can be addressed through the SPI connection similar to the ATA8350 UWB device. The ATA8352 UWB device register bits are grouped into the following categories:
  • A: Fixed value, no changes required
  • B: Value to be defined once, at the HW end-of-line testing
  • C: Value to be set up every time the system starts
  • D: Value that defines the Operating modes and parameters
Note: It is highly recommended to check the register descriptions in both the ATA8352 and ATA8350 UWB devices to determine the changes.

For more details about the register description, refer to the ATA8350 Impulse-Radio Ultra-Wideband (IR-UWB) User Guide and ATA8352 Impulse-Radio Ultra-Wideband (IR-UWB) User Guide.