The following figure illustrates the overview of a schematic for the ATA8352 UWB device. Some
components are marked as not mounted (red color cross), as they are not necessary for
describing the application use for demo, and TDoA. In comparison to the schematic of
Figure 3-6, there are plenty of changes in the
BOM. For example, the C6 capacitor quantity changes from 3.3 pF in the ATA8350 UWB
device to 1.4 pF in the ATA8352 UWB device. A DC/DC converter is not mounted in the
ATA8352 module schematic, as illustrated in the following figure. For more details,
refer to the ATA8352 Demo and Evaluation Kit User’s Guide and ATA8350 Demo
and Evaluation Kit User’s Guide.Figure 3-5. ATA8352 Module Overview
Schematic
Figure 3-6. ATA8350 Module Overview
Schematic
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.