Description
This Tcl command sets the maximum TCK frequency of a non-Microchip device in the chain. Chain
programming mode must be set. The device must be a non-Microchip device.
set_device_tck -name {name} -tck {tck}
Arguments
Parameter | Type | Description |
---|
name | string | Specifies the non-Microchip device name. |
tck | decimal | Specifies the maximum TCK frequency (in MHz). TCK frequency be greater than or equal to 1.000 and less than or equal to 100.000. |
Return Type | Description |
---|
None | None |
Error Codes
Error Code | Description |
---|
None | Required parameter 'name' is missing. |
None | Required parameter 'tck' is missing. |
None | Parameter 'tck' must be greater than or equal to 1.000. |
None | Parameter 'tck' must be less than or equal to 100.000. |
None | Parameter 'tck' has illegal value. |
None | tck: Invalid argument value: '' (expecting decimal value). |
None | Parameter 'name' has illegal value. |
None | Parameter 'param_name' is not defined. Valid command formatting is 'set_device_tck -name "name" -tck "decimal value"'. |
Supported Families
Supported Families |
PolarFire® |
PolarFire SoC |
RTG4™ |
SmartFusion® 2 |
IGLOO® 2 |
Example
The following example sets the maximum TCK frequency of the non-Microchip device 'MyDevice':
set_device_tck -name {MyDevice} -tck {2.25}